AXIS#.MT.MOVE
Description
This command needs one argument in order to start a motion task. The drive must be homed, otherwise the motion task will not start.
Example
AXIS#.MT.MOVE 3 -> Start motion task number 3.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-00-00-000 | |
General Information
This content is not applicable to KAS.
Type |
Command |
Units |
N/A |
Range |
0 to 31 |
Default Value |
N/A |
Data Type |
N/A |
Stored in Non Volatile Memory |
No |
Variants Supported
All variants are supported.
Related Topics
Motion Tasks